10/1/2019 5:36 PM | |
Posts: 672 Rating: (57) |
Hi, Quotation marks? "INPUT" Pee |
10/3/2019 5:22 AM | |
Posts: 3 Rating: (0) |
We tried with Quotes . But still it is not working |
10/3/2019 9:11 AM | |
Joined: 5/24/2016 Last visit: 9/13/2024 Posts: 347 Rating: (52) |
Which PPU verision of 828D do you have?? |
10/3/2019 10:50 AM | |
Posts: 3 Rating: (0) |
PPU 271.4 |
10/3/2019 2:14 PM | |
Joined: 5/24/2016 Last visit: 9/13/2024 Posts: 347 Rating: (52) |
Hello. I just tried your configuration in Sinutrain with the changed i mentioned above, and that works fine. How is your easyscreen.ini file configured and how did you configure the .com file? This i the code in the video //S(START) //M("WELCOME TO HMT MTK MACHINE ") HS7=("Input/Output%nDetails") PRESS(HS7) LM("Maske6") END_PRESS //M(maske6/"INPUT/OUTPUT OF SBCNC 30 Y AXIS") HS9=("INPUT") HS10=("OUTPUT") PRESS(HS9) LM("Maske7") END_PRESS PRESS(HS10) LM("Maske8") END_PRESS //END Best Regards Riddersholm AttachmentEasyScreen.avi (53 Downloads) |
Follow us on