10/5/2019 9:33 AM | |
Posts: 89 Rating: (0) |
{snip} Please see attached screenshots. Does it look ok? And im trying to use address IW304? EDIT: What is PIW304? ------------------------------------------------------------------------------------------ |
Last edited by: Garrianz at: 10/05/2019 09:34:34Last edited by: The Helping Hand at: 10/08/2019 10:16:26New subject after splitting Last edited by: The Helping Hand at: 10/08/2019 10:18:06Removed reference to original thread. |
|
10/5/2019 9:33 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
Try to read the address not of IW304, but of PIW304. |
10/5/2019 9:49 AM | |
Posts: 89 Rating: (0) |
Thank you so much, I will try this out soon. I thought s7-300 was a powerful PLC? Why the low IO memory? |
10/5/2019 9:52 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
For periheral addressing - check this. Some CPUs allow to increase size - see attachment. Increasing the size of the "Process image" increases the CPU cycle time. In the 90s and 00s, it really was powerful. Now the trend is S7-1500. |
Last edited by: Konstantin_D at: 10/05/2019 10:09:10 |
|
10/5/2019 10:22 AM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
There are two functions for working with analog signals:
|
Follow us on