9/17/2019 3:11 PM | |
Posts: 8 Rating: (0) |
Hi I have connected some G120 VFDs to 1500 cpu by Profinet. Also I have used Technology Object> Motion Control to control them. Simultaneously I am going to change the torque limit of drive during operation. As I understood to have torque control by Motion Control, it is needed to set the drive on Telegram 10x, but the CU250S doesn't support it. Firstly I want to know is it correct or not? Is there any way? Finally I have used SINA_PARA function for sending torque limit value to the drives (simultaneously control them by Motion Control). But unfortunately after a while the torque limit value doesn't send to the drive and it is needed to turn on and off the PLC or STOP/RUN. It seem there is a communication problem. however the speed control is working. I prefer to monitor some parameters during operation of drive. Would you please help me. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/18/2019 08:16:54New subject after splitting |
|
10/4/2019 12:24 PM | |
Posts: 8 Rating: (0) |
Hi Do you mean here in attached picture? How can I get good knowledge about Telegram? Thank you |
Follow us on