10/4/2019 5:36 PM | |
Joined: 4/29/2017 Last visit: 5/10/2024 Posts: 47 Rating: (1) |
Hi Friends, I installed wincc on my pc With on oracle Virtual box But after installation when Clıck wincc Explorer on desktop ,İt doesnt work sometimes its opening but usually not What is the problem any idea? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/07/2019 09:40:52New subject after splitting |
|
10/4/2019 5:57 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (81) |
Hi One things to do, is to check the logs files. You will find it, C:\Program Files (x86)\Siemens\WinCC\diagnose If you are running over virtual machine, you have to assing at least 4GB RAM - 8 much better ;-) and the service SQL Server must be running. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
10/7/2019 10:16 AM | |
Joined: 10/26/2005 Last visit: 5/10/2024 Posts: 282 Rating: (48) |
Hello, I would guess that you have no network enabled. Add a NIC with windows networking enabled. //PerD |
7/16/2021 7:55 PM | |
Joined: 8/24/2018 Last visit: 5/3/2024 Posts: 19 Rating: (0) |
Question just using VM Workstation will not work as well? |
Automation is about making things talk |
|
Follow us on