10/9/2019 8:18 PM | |
Joined: 9/30/2013 Last visit: 4/26/2023 Posts: 4 Rating: (0) |
Hello, I am using the last v2.4 example image and am trying to install modbus and netpie package but to no avail. I performed the procedures as the site https://support.industry.siemens.com/tf/ww/en/posts/tip-installing-nodes-on-iot2000/180905/?page=0&pageSize=10 with the codes npm -g install node-gyp node-gyp install and others. I used the codes below to install modbus packages 1- cd / usr / lib / node_modules npm install node-red-contrib-modbus 2- npm install -g node-red-contrib-modbus 3- npm install node-red-contrib-modbus@3.6.1 --unsafe-perm --build-from-source 4- npm install node-red-contrib-modbus@2.5.0 --unsafe-perm --build-from-source I used the code below to install the netpie package npm install node-red-contrib-netpie All the codes generated an error, I don't know what else to do, can anyone help me? I used this code "date MMDDhhmmYYYY" (Month: Date: hour: minutes: Year) to add the date. NODE.JS VERSION 6.14.3 i use dns google 8.8.8.8 8.8.4.4 /etc/resolv.conf The rest of the error in the annex ------------------------------------------------------------------------------------------ AttachmentError.zip (113 Downloads) |
Last edited by: Alisson934 at: 10/09/2019 21:05:16Last edited by: Alisson934 at: 10/09/2019 23:01:21Last edited by: The Helping Hand at: 10/10/2019 12:38:19New subject after splitting |
|
10/10/2019 1:20 PM | |
Joined: 8/21/2014 Last visit: 4/24/2024 Posts: 951 Rating: (13) |
Closed because question was posted twice. Please use: Modbus RTU node installation problem |
My Forum is the place to personalize your profile, |
|
Follow us on