10/2/2019 8:04 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hi I would like to ask, if you are working with WinCC v7.5 and the last update 4 if for your the function Logout works correctly. I have some trouble and I don´t know if the problem is the installation or a bug. I have tested severals instalation over virtual Machine and the real IPC I have use the code with ANSI C ,
By the way I have tested with the shortcut of the project properties and nothing... Can you share your testing? PD. I don´t see nothing in diagnose folder... Thank you Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
10/4/2019 10:39 AM | |
Joined: 5/21/2018 Last visit: 11/29/2023 Posts: 16 Rating: (2) |
I use 7.5 update 4 and seems working fine. See attached SS. |
This contribution was helpful to1 thankful Users |
10/4/2019 1:47 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hello Georg Firts, Thank you very much for your feedback!!! :-) I have check all the diagnoses files and windows logs, and I don´t find anything wrong. But don´t works. I don´t have the Audit installed. Do you have another suggestion? Thank you Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
10/4/2019 1:50 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Hello DK Thank you very for your feedback. Did you try the Runtime? For me, the Login function works fine, I have trouble with Logout. Thanks Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
10/10/2019 9:34 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Thank you very much for your feedback. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
10/24/2019 2:26 PM | |
Joined: 11/14/2016 Last visit: 4/23/2024 Posts: 1 Rating: (0) |
HI PHS Your WinCC is redundancy server? |
Follow us on