2/22/2018 5:28 AM | |
Posts: 3 Rating: (0) |
Hi, Please Help me, I want to do upload of the S71200, but I have in library V4.1; and the PLC is V4.1.1. I think that is the problem I don´t can upload program; I think that I need HSP 6ES7214-1AG40-0XB0_V4.1.1??,...Where Can I download it?? I have Tia Portal V13 SP1 Update 9 Thanks For your help!! ------------------------------------------------------------------------------------------ |
Last edited by: poolsmith at: 2/22/2018 5:30:03 AMLast edited by: Jen_Moderator at: 2/22/2018 12:16:14 PMNew subject after splitting |
|
5/14/2018 11:33 AM | |
Posts: 1 Rating: (0) |
HI, I have the exact same problem... Did you managed how to solve it? Thank you |
10/11/2019 9:03 AM | |
Posts: 1 Rating: (0) |
I have the exact same problem... Help, please. Thank You |
10/18/2019 8:44 PM | |
Posts: 5 Rating: (2) |
I am also facing the same "Not compatible'' issue, -i have 1214dc/dc/dc with firmware 4.1.3, i want to upload program and hardware configuration of this cpu for backup purpose. -i have installed tia portal v13 sp1 with update9 in my laptop and tried connecting above mentioned cpu with my laptop. -in online access i m able to detect cpu and able to view program blocks, than i have defined unspecified cpu in project and clicked on DETECT button to upload hardware in Tia project and that is successful uploaded -but when i m triying to go online with the project configuration it refuse to get online, Information window shows connection terminated and in online diagnostic window it displays not compatible, and in diagnostic status window it says not supported - there are no firmware 4.1.3 in my tia portal for s7-1214, only 4.0 and 4.1 is available to define - all photos attached - thanks in advance
Attachmentnot compatible photo.zip (366 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on