10/8/2019 9:32 AM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating: (68) |
Hello Sampathkumar007s, regarding simulation, there is an application example which might help you further. Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
This contribution was helpful to1 thankful Users |
10/11/2019 1:09 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
HelloSam first of all we should clear if you need a Station configuration on the Runtime PC (Simatic Net with Station configuration) or not. IF you just want to Run the WInCC Professional RT on the PC without using Simatic NEt OPC Server or Soft PLC or something else you must load to the PC Station then you only have to install the Simatic Net on the Runtime PC for the Communication drivers. you do not have to set something in the Simatic Net Settings. In the TIA Portal Project just create a PC Station and an IE general Card for the Process Communicaiton with the PLC (for the HMI Connection in the Project) Then use the following two FAQs to setup your PC Station and load the Project to the RT Station: https://support.industry.siemens.com/cs/de/en/view/108464289 https://support.industry.siemens.com/cs/ww/en/view/88780011 (https://support.industry.siemens.com/cs/ww/en/view/87054082) Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on