10/9/2019 9:31 AM | |
Joined: 9/8/2019 Last visit: 12/16/2021 Posts: 54 Rating: (0) |
Hi everyone , I need to connect logo8 To a SCADA System (((over internet)) Because Scada and the logo (((are not at the same place )))) How i can do this connection in details ((hardware and software)))??? thank you in advance :) ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/09/2019 10:02:28New subject after splitting |
|
10/9/2019 9:33 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Are the LOGO! and the SCADA not in the same subnet, the you have to use a gateway e.g. a router |
10/9/2019 11:11 AM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
If you have a SCADA system which can communicate with the Logo8 over LAN, then it is the easiest way to use VPN. If you need specific answers then use specific questions. Regards, Scorp |
10/9/2019 3:39 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
As Scorp wrote: More details please. Your questions is to generell. What mean you with Ethernet? A company network? Or are the places spatially so far apart that you have to go over the public internet? And please consider: If you help from Siemens directly, start a Support Request of contact your loacal Siemens Office. |
Follow us on