10/14/2019 2:16 PM | |
Joined: 10/11/2006 Last visit: 5/3/2024 Posts: 5832 Rating: (789)
|
Hello, you cannot upload DCC charts with Startdrive, if the charts were created with Starter. In this case, the charts are not load to the PC. You can export the charts in Starter to .xml and import these into the Startdrive project (e. g. after the upload without the charts). If your chart contains multiple runtime groups, you need to follow these steps in Starter before exporting to .xml: https://support.industry.siemens.com/cs/ww/en/view/109764320 |
With best regards, |
|
This contribution was helpful to2 thankful Users |
Follow us on