1/25/2017 5:09 PM | |
Joined: 3/21/2013 Last visit: 9/20/2017 Posts: 1 Rating: (0) |
Hello. I am installing a system on a Windows 7 Pro SP1 x64 system with:
I tried to follow all the indication. I installed the software package without any error. I Login to Windows with the same Administrative user of the installation (User in all the Siemens groups). I open the Internet Explorer and introduce "localhost" or the "Server Name" and LOGIN to IS portal. But after the successful login, appear an ERROR: "Your secession lacks an interactive permission required to run setup. It is recommended that you run Microsoft Internet Explorer locally on the Server. in that case you must also ensure that automatic user authentication is being used, i.e. no login popup is being shown when you access this website." I followed the indication and configure the Internet Option with: "Prompt for user name and password."; but after the Error message, I modified that to "Automatic logon only in Intranet Zone". What can I do? How can I solve this issue? Thank you. Regards, Paul ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/26/2017 3:54:09 PMNew subject after splitting |
|
7/24/2017 11:29 AM | |
Posts: 4 Rating: (1) |
In Internet Option -> Security -> Custom level -> Allow the option "Login with current name and password". |
4/23/2019 12:53 PM | |
Posts: 1 Rating: (0) |
its not done with this setting please provide some other path |
12/29/2020 3:18 PM | |
Joined: 4/28/2015 Last visit: 12/14/2023 Posts: 1 Rating: (0) |
I am having the same problem now, Can anyone give support? |
Follow us on