10/14/2019 10:55 AM | |
Joined: 11/14/2018 Last visit: 10/31/2023 Posts: 502 Rating: (68) |
Hello shoaibb95, as a first step to start with, I would suggest this FAQ and the included documentation: It discusses the Sm@rtServer functionality for Industrial Thin Client, but like I said, it may serve as a starting point for you. Greetings, Nzett11 |
If I could help you, be so kind and rate my contribution. :) |
|
10/15/2019 10:21 AM | |
Joined: 6/20/2018 Last visit: 4/12/2024 Posts: 18 Rating: (0) |
I think I did exactly same but couldn't make it work, on some research found out that I can access HMI over internet through port forwarding, but since I'm a *** in networking so stuck! |
10/21/2019 7:45 AM | |
Joined: 6/20/2018 Last visit: 4/12/2024 Posts: 18 Rating: (0) |
I've attached a pdf file which contain all the things I did so far, if any one can look into it, it'd be really helpful for me :)
AttachmentRemote Monitoring Over Internet.pdf (154 Downloads) |
10/22/2019 3:11 PM | |
Joined: 8/3/2009 Last visit: 4/19/2024 Posts: 12816 Rating: (1634)
|
Helloshoaibb95 There are some Information in this FAQ: https://support.industry.siemens.com/cs/de/en/view/109476153 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on