10/14/2019 12:19 PM | |
Posts: 4 Rating: (0) |
Hello, I have an S-120 CU310-2 PN, FW V5.1.0.2 that is installed and running. I want to access the parameters of the Drive but I get to "Accessible Nodes" and I get the screen shown in attachment. My Starter is V5.3.0.3. I have downloaded the SSP's that I could find but may not have installed them correctly. Help is much appreciated. Attachmenterror.docx (233 Downloads) |
Last edited by: ringneck at: 10/14/2019 12:29:08 |
|
10/14/2019 12:29 PM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
hello, which ssp you have downloaded and installed? https://support.industry.siemens.com/cs/attachments/109477641/SSP_SINAMICS_V5_1_HF3.zip or copy the ssp setup from the compatctflashcard. the path is listed in accessible nodes. regards christoph |
10/14/2019 8:07 PM | |
Posts: 4 Rating: (0) |
Christoph, Please see attached file for installed devices. The download site showing extracting and installing is very confusing to me. Best Regards, - Scott Attachmentinstalled devices.docx (223 Downloads) |
Last edited by: ringneck at: 10/14/2019 20:08:22Last edited by: ringneck at: 10/14/2019 20:10:28Last edited by: ringneck at: 10/14/2019 20:10:57 |
|
10/15/2019 12:24 PM | |
Posts: 4 Rating: (0) |
Thank you Christoph, I will try this when I return to work in 1 week. - Scott |
Follow us on