10/17/2019 10:15 PM | |
Joined: 12/18/2014 Last visit: 5/9/2024 Posts: 32992 Rating: (4077) |
Which function has %S13 by Twido? |
10/18/2019 12:34 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
I have put the project to pdf its only 11 rungs of code. I think the code is based similar to schneider PL7 it refers to this as a system bit......First cycle after switching to RUN Normally at 0, is set to 1 by the system during the first cycle after the PLC switches to RUN. I have coded using Tia portal v15 but have not included the system bit %s13 from the original code Ade AttachmentSS2_Marlboro_CAT2_V1.pdf (33 Downloads) |
10/18/2019 2:32 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Google search produced a reference guide that shows %S13 as a system bit, specifically a "First cycle in RUN". The equivalent to that is "How can you avoid...." |
Last edited by: Jen_Moderator at: 10/18/2019 11:34:28Optimized link. |
|
This contribution was helpful to2 thankful Users |
10/18/2019 9:33 AM | |
Joined: 11/15/2017 Last visit: 9/2/2022 Posts: 87 Rating: (0) |
Hello, As a relative newcomer to TIA I would like to thank you for your guidance Ade |
Follow us on