10/17/2019 1:30 PM | |
Posts: 9 Rating: (0) |
Thank you everybody! I resolved my problem! The parameter P3900 was 0. I chose P3900=3 and after that P0010=0 (Ready). One problem is finished. After quick comissioning and motorID I click the start button. IOP shows an icon of motor but after 10 seconds I get fault F07802: Drive: Infeed or power unit not ready. DC voltage is OK. p0857=10 sec p0210=400V anybody know this problem ? Regards, Stan! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/18/2019 09:33:33New subject after splitting |
|
Follow us on