10/18/2019 11:49 PM | |
Joined: 8/4/2014 Last visit: 1/29/2024 Posts: 23 Rating: (1) |
Dear all, I have a question about upgrading FW on CU320-2 PN. ACTUAL CONFIGURATION: 1) Control Unit: CU320-2 PN 6SL3040-1MA01-0AA0 2) Control Unit FW: 4.8.0.5 3) Commissioning tool: Starter V5.3.+HF3 4) Starter project version: V4.8 5) DCC charts technology package version: V4.80.11.0 6) CF card hardware number: 000060147054A6000062 7) CF card order number: 6SL3054-0EJ01-1BA0 8) CF card license number: T-K8IL05886 In order to be able to use TIA Startdrive V15.1 as a commissioning tool I need to update FW on control unit from V4.8. to V5.2. by following this instructions: https://support.industry.siemens.com/cs/ww/en/view/109762626 After updating FW on CU I will update Starter project versions from V4.8. to V5.2. and download them to CU. Next thing to do is to update technology package for DCC charts from V4.80.11.0 to V5.10.8.0. After updating project and DCC versions, I have to convert them to Startdrive versions following steps on this link (I have only one execution group): https://support.industry.siemens.com/cs/ww/en/view/109764320 QUESTION: How can I know if actual license on my CF card will support new FW version (I will save active keys)? I have used Web License Manager to check status of my actual license, but there are no any information about which FW versions are supported with actual license key. Maybe I'm asking stupid question, but before doing all of mentioned jobs above, I would like to be sure that actual license will support new FW version and new technology packages for DCC, and once projects are migrated to TIA Startdrive to not have warnings about not valid license keys... Thank you for support! |
Last edited by: Jen_Moderator at: 10/21/2019 08:40:30Optimized links. |
|
10/21/2019 12:35 PM | |
Joined: 10/11/2006 Last visit: 5/3/2024 Posts: 5832 Rating: (790)
|
Hello, |
With best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on