10/19/2019 8:52 AM | |
Joined: 8/10/2016 Last visit: 2/18/2024 Posts: 16 Rating: (0) |
Dear Expert, I have try to create S7 Communication project using S7-1200 PLC. In this project i found error, kindly see the attached DIAG.I have active the GET/PUT connection. For your kind information, i found this error during simulation and if i use NC contact for REQ get/put instruction instead of clock memory 1HZ that time Error gone. But communication not established. Project Link: [snip] Note: In this project Send RCV DB are empty. I filled it and tried still same error. Kindly help to resolve the issue. Best Regards, Farhan Rajib AttachmentFiles.zip (39 Downloads) |
Last edited by: DarkSpike at: 10/19/2019 08:54:32Last edited by: DarkSpike at: 10/19/2019 11:32:14Last edited by: DarkSpike at: 10/19/2019 11:56:35Last edited by: Jen_Moderator at: 10/21/2019 09:02:44Removed links and added files as an attachment. |
|
Follow us on