10/21/2019 9:17 AM | |
Joined: 10/3/2013 Last visit: 10/26/2023 Posts: 123 Rating: (3) |
Hi, 1. Will any one explain how we configure ET200SP HA with As-410H by activating R1 Redundancy mode? What will be steps the to activating R1 Redundancy mode in AS-410H? I have gone through various manuals which makes some confusion. 2. We have IO et200sp ha io system with two Im & some IO modules foe redundant R1 mode with CPU 410H. But we have to configure only standalone AS-410 cpu with one IM for some testing purpose. Is it possible in existing hardware without removing second IM. Also I have attache word file to explain it. AttachmentSys.docx (77 Downloads) |
10/21/2019 12:40 PM | |
Joined: 9/3/2013 Last visit: 11/3/2023 Posts: 152 Rating: (31) |
Hello Mahesh, for your first question i recommend this: https://support.industry.siemens.com/cs/ww/en/view/109747703 e.g. chapter 2.1.2 About your second question: "We have IO et200sp ha io system with two Im & some IO modules foe redundant R1 mode with CPU 410H. But we have to configure only standalone AS-410 cpu with one IM for some testing purpose." What are you trying to do / to test? If you configre the System as single System you have to recreate the HW-Config afterwards. theoretically you can configre your whole system as H-System with R1 redundancy and test things with one site, while the other is missing. Greetings |
Last edited by: Technodrome at: 10/21/2019 13:02:27Last edited by: Technodrome at: 10/21/2019 13:37:05 |
|
11/6/2019 7:22 AM | |
Joined: 10/3/2013 Last visit: 10/26/2023 Posts: 123 Rating: (3) |
Thanks. I have done same. Still IO's are blinking.
Is there any liscene in AS is required for ET200 SPHA R1 configuration? If yes, How it will get activated or transfer into the CPU? Thanks |
Follow us on