10/21/2019 5:01 PM | |
Joined: 5/2/2015 Last visit: 3/21/2024 Posts: 1 Rating: (0) |
Hello there try switching your windows 10 language back to english
|
11/8/2019 1:15 PM | |
Joined: 11/7/2019 Last visit: 4/16/2024 Posts: 7 Rating: (1) |
Hello all. I see there are many posts about this issue of installing TIA V15.1 but the particular error in this thread is the closest to the problem I am having so I'm going to tag onto this. I'm a complete Siemens *** so I could be missing something very simple. I've attached my install log file for review. The error(s) I get is: 14:04:52 |ERROR AdsWorkerClassicProduct::OnWorkerCompleted(): - ClassicProduct setup result: 170: Info: SQL Installation was not Successful 14:04:52 | FAIL! SetupUnit (INSTSQL2014EXP) Failed ClassicProductAddLocal 14:04:52 | FAIL! Checkpoint (E) Complete 14:04:52 |ERROR ExecutionEngine::StartNextStepAsync(): - Execution has been cancelled. Probably because of some process(es) running on the machine I was working with one of my MIS colleagues yesterday to try and figure this out but we couldn't so any suggestions to try would be appreciated. Thanks in advance AttachmentSIA_STEP_7_PRO_WINCC_ADV_V15.1@19-11-07_13-52-58_summary.txt (392 Downloads) |
11/8/2019 2:58 PM | |
Joined: 11/7/2019 Last visit: 4/16/2024 Posts: 7 Rating: (1) |
Update on my issue: I uninstalled the virus protection software on my PC completely and tried to reinstall TIA and now have a different error. Log file is also attached. So now I've also tried turning off windows defender and I've stopped any factorytalk services as well as any service related to SQL but still have this error: ERROR AdsWorkerClassicProduct::OnWorkerCompleted(): - ClassicProduct setup result: 52: Info: SQL Installation was not Successful 08:52:34 | FAIL! SetupUnit (INSTSQL2014EXP) Failed ClassicProductAddLocal 08:52:34 | FAIL! Checkpoint (E) Complete 08:52:34 |ERROR ExecutionEngine::StartNextStepAsync(): - Execution has been cancelled. Probably because of some process(es) running on the machine
AttachmentSIA_STEP_7_PRO_WINCC_ADV_V15.1@19-11-08_08-50-49_summary.txt (340 Downloads) |
11/8/2019 7:47 PM | |
Joined: 11/7/2019 Last visit: 4/16/2024 Posts: 7 Rating: (1) |
Thank you StefanoZ. That worked. I think the issue comes in to play where the TIA is trying to install a SQL service where there already is one. Here's a response from a customer service rep on the issue: Most likely, the issue related to an instance of the SQL 2014. This is must be deleted. Once deleted, run the install of V15.1 again. It will put the instance back. Attached is Word document with some steps of removing the instance. Please be patient. It may take some time for uninstall dialogue to appear. I am going to uninstall and try this as well and see if i can run the install with the migration tool included. AttachmentWINCC_MIG_2014.docx (855 Downloads) |
This contribution was helpful to1 thankful Users |
8/21/2020 1:44 PM | |
Posts: 1 Rating: (0) |
Download install SQLEXPR_x86_ENU and no problem |
Last edited by: reshacker777 at: 08/21/2020 13:45:12Last edited by: reshacker777 at: 08/22/2020 13:30:24 |
|
6/1/2021 8:03 AM | |
Joined: 8/12/2018 Last visit: 11/18/2021 Posts: 1 Rating: (0) |
M also facing same issue. My OS is Windows 10 Professional 64-Bit |
Follow us on