4/29/2019 12:23 PM | |
Joined: 11/29/2011 Last visit: 8/19/2024 Posts: 1359 Rating: (232) |
Hi, Only @CPU @ chart exist. If I delete that it does not make any difference. Anyways I noticed a warning in log. "(---) Not Supported" See the attachment. Attachment20190429_Module driver.txt (450 Downloads) |
- What you read here, please check with manuals and your requirements. |
|
4/29/2019 8:37 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi MicroMan, Can you give me some more info like: - MLFB number of the configured Simocode slave and it's modules - The used driver blocks in CFC chart (please attach a print screen also) - Are you using PCS7 V7.1 without service packs? And Simocode pro V7.0 Upd2 correct? - GSD file name of the Simocode slave I will investigate this further. It looks like some hardware configured is not supported by the system. |
If I could help you, you can use the RATE button. Thank you. |
|
4/30/2019 3:30 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi MicroMan, According to the manual, you are using the correct MLFB and GSD file. Are the defined inputs/outputs of the Simcode slave within the process image of the CPU? I saw your other post of the supporting CPU. Is this CPU released for PCS7 V7.1? That maybe a problem if it is not and could be related to your issue with Simocode. What if you create a copy of the multiproject and replace the CPU by a released CPU? Please select PCS7_V71 catalog instead of Standard catalog in hardware configuration to see the released modules. MicroMan: Did you do a proper update? I mean, did you mix different versions of driver blocks for example? If there are different versions, it may be that the system returns errors , please check if libraries are updated correctly and not mixed |
Last edited by: Oreca at: 04/30/2019 17:28:44If I could help you, you can use the RATE button. Thank you. |
|
2/10/2023 10:22 AM | |
Joined: 8/21/2020 Last visit: 11/3/2023 Posts: 1 Rating: (0) |
Thanks for your help. |
Follow us on