10/23/2019 9:11 PM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
You can use the function from the menu Online -> Download to file system. More details. |
This contribution was helpful to1 thankful Users |
10/25/2019 12:25 PM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello Anna Is you problem solved now? If not then please describe a little bit more detailed? If you have a live connection to the Runtime System then you can also use this FAQ: https://support.industry.siemens.com/cs/ww/en/view/88780011 Bye Murof |
If this Information really helps, you could use the Rate function |
|
10/25/2019 1:10 PM | |
Joined: 8/28/2019 Last visit: 6/13/2022 Posts: 18 Rating: (1) |
Hello, yes it is solved, I used Online -> Download to file system |
Follow us on