10/3/2019 2:05 PM | |
Joined: 1/14/2014 Last visit: 8/5/2024 Posts: 15 Rating: (0) |
Hi, I'm using the latest Example_Image_V2.4.0.zip (365,0 MB), but every time i try to install the OPC UA node i get the following error:
Could someone please help me? |
10/3/2019 2:16 PM | |
Posts: 9 Rating: (0) |
bump - Having same issue |
10/7/2019 10:32 AM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, are you able to see the OPC UA nodes after the installtion in node-red? Maybe your problem could be solved with this: https://support.industry.siemens.com/tf/ww/en/posts//197625/ Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
10/7/2019 1:58 PM | |
Joined: 1/14/2014 Last visit: 8/5/2024 Posts: 15 Rating: (0) |
Hi! The problem is, that the actual version of node-red-contrib-opcua is no more compatible with the nodeJS 6. But i cannot upgrade the nodeJS on the IOT2000 because it's CPU is not supported anymore. So i was able to install the version 0.2.11 but it has a strange behavior when i subscribe to an opc ua variable. After a few poll, it goes to error and cannot reconnect (2 sec polling). [error] [OpcUa-Client:id] id OPC UA connection error: Transaction has timed out Any idea? Which is the most recent version of this node that I am able to install on the IOT2040 without any incompatibility?
|
Follow us on