11/4/2008 3:36 AM | |
Joined: 9/27/2006 Last visit: 9/19/2024 Posts: 12282 Rating: (2684) |
Hello faming; Sorry, I don't have access to Step 7 at this moment, so I couldn't see the details of your configuration. So if this comment is not useful, please accept my apologies. Basically, to my knowledge, the "replace during operation" function is a slave property that you setup in the ET 200M parameters. Is this something you have taken into account? The following FAQ shows a screenshot of the required configuration, and discusses theactive bus modules required for the operation: http://support.automation.siemens.com/WW/view/en/29108474 Hope this helps, Daniel Chartier |
11/5/2008 3:36 AM | |
Joined: 6/8/2007 Last visit: 9/3/2024 Posts: 41 Rating: (1) |
thank you for your answering . |
11/5/2008 5:45 PM | |
Joined: 7/2/2008 Last visit: 8/26/2024 Posts: 928 Rating: (308) |
Dear J_Bell, I've just foundthe FAQ I was pointing at. I did that test about 4 months ago and I really can't remember the part no. of the ET200M. But if I havethe latest IM153-2 and configured it with its GSD file, will it support Acyclic communication even though it is configured with GSD file? And if it works with Acyclic communication, Do you thinkhot swappingmight work without that short break in outputs? |
Follow us on