11/5/2019 7:27 PM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (42) |
Hi all, I would like to set a bit when I open a pop-up, and reset it when the pop-up is closed. The set part works great, but when I choose to reset the bit at the cleared event, it is immediately reset. I can probably find a way around the issue, but what exactly is the cleared event for a pop-up? The HELP says: Occurs when the active screen on the HMI device is cleared. This doesn't really clarify the issue...Thanks! edit: after some more investigation, it seems that the bit is set correctly, but when I navigate from one pop-up to the next, it is resetting the bit. |
Last edited by: Ton Verra at: 11/05/2019 19:48:36 |
|
Follow us on