11/7/2019 3:44 PM | |
Joined: 11/20/2017 Last visit: 4/19/2024 Posts: 7 Rating: (0) |
Hello schufri, Thanks for the reply. The authorizations are not relevant, as they are not specified in HORN configuration. The configuration follows attached. It works fine but, as I said, I don't know if it is normal to activate the Horn on user login. After reading the "Minimal Horn Configuration" carefully, I found an info that states if "no authorization has been specified, there is also a check wheter a signal is triggered". So, I believe that when a user logs on, regardless of its authorizations, this alarm check takes place and if positive it triggers the horn. In the attachments, CMD_ACTIVATE_HORN is the external signal tag, that when positive it sets HORN_ACTIVE, another external tag. AttachmentHORN Configuration.pdf (314 Downloads) |
Follow us on