11/12/2019 9:00 AM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (106) |
Hello Martyndwn3, only thing what I see is that they got same ID, host and partner, I don't think this is allowed. S7 communication inside PLCSIM should be allowed, there should be no problem because of that Yo have here S7 communication in between two or more S71500, even project has been attached: Multiple S71500 S7 communication Best Regards Soble |
Last edited by: SOble at: 11/12/2019 09:02:01Website: |
|
11/12/2019 9:01 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
Hello, here is a FAQ for this topic: https://support.industry.siemens.com/cs/ch/en/view/88781327 Regards |
11/12/2019 9:54 AM | |
Joined: 9/13/2019 Last visit: 5/10/2024 Posts: 2 Rating: (0) |
Thank you everybody, Following the steps in the link provided seems to have solved it https://support.industry.siemens.com/cs/ch/en/view/88781327 The local and partner ID's are all the same, which is a little confusing, but it doesn't have any errors. Thanks again. |
Last edited by: Jen_Moderator at: 11/12/2019 11:32:35Optimized link. |
|
Follow us on