11/6/2019 10:50 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Sorry for the late reply but we have no experience with this module. In my opinion Telit themselves should provide such a script for configuration. From what their manual says, if the device is recognized correctly, you should use either /dev/ttyACMx or /dev/ttyUSBx as serial port for configuration. This is normally something ppp handles for you and is also part of this application example. |
11/13/2019 1:04 PM | |
Joined: 3/27/2017 Last visit: 9/17/2024 Posts: 24 Rating: (2) |
I just made it work, in this case ppp was not enough, because I needed to set the board before so I could make some tests. I did a step by step if anyone face the same issue
AttachmentAT_Commands.pdf (172 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on