11/12/2019 6:06 PM | |
Joined: 2/1/2010 Last visit: 4/24/2024 Posts: 131 Rating: (66) |
Hi ashadako, On my PCS7 9.0 SP1 and SP2 install systems I have both the block icons in the @PCS7TypicalsV8.pdl and faceplates in the GraCS folder for S and L blocks. I did find on the SP1 system that the @PCS7TypicalsV8.sav file is missing the L block like you are. I'm thinking that this may be patched in from an update and is missing if you migrated your project from an earlier version. You might be able to recover the correct @PCS7TypicalsV8 into your project from the master folder: C:\Program Files (x86)\SIEMENS\WinCC\Options\PDL\APL. (Running OS Project editor should do this for you if you can do that, or you can copy manually) Do you have the faceplates in your GraCS folder and only missing the block icon? Let me know if that helps. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to1 thankful Users |
11/13/2019 2:17 PM | |
Joined: 2/1/2010 Last visit: 4/24/2024 Posts: 131 Rating: (66) |
Based on your screenshots I can see your OS project has not been updated with the correct copies of the block icons and faceplates. You need to complete the migration correctly by completing OS Project Editor (Just press OK button on the second screenshot you sent and it will copy all the files from the master files into your project). If somehow that is not working then just copy the all files manually probably including emf, png files etc (Not Open them, copy to your project folder - all OS stations projects) from the master folder location I posted earlier. Opening graphics directly from the master folder will always lead to strange visual problems because the emf files are losing their reference when opening from that location. This answers the other post you opened about this file. The APL library has two "generations" V7 and V8. The V8 generation of blocks (while still gaining new features in every version including 9.0 SP2) is still the primary lineage of PCS7 V9 APL. It is normal that @PCS7TypicalsV8 is the file you want. |
Last edited by: RVS.wick at: 11/13/2019 14:19:27Last edited by: RVS.wick at: 11/13/2019 14:23:32If my post helped you, please rate. Thanks. |
|
This contribution was helpful to2 thankful Users |
Follow us on