11/13/2019 3:46 PM | |
Joined: 3/25/2008 Last visit: 4/25/2024 Posts: 182 Rating: (7) |
hello, put into trace n set (K170), n act (K167), I act (K115), adjust speed contlollerr P225, P226
|
11/28/2019 5:23 AM | |
Posts: 95 Rating: (0) |
thanks sir |
11/28/2019 6:07 AM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22228 Rating: (2980) |
Hello, use another adapter. For Masterdrive the Aten UC232A should be work.
Christoph |
11/29/2019 5:20 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
What was fault in motor? Was armature rewinding or field rewinding carried out? Please discuss with vendor get fault data & repairs work information.
Please refer SIMOREG DC-MASTER 6RA70; software version 3.1 manual, chapter 7.5 Start up procedure, topic 8 execution of optimisation run. Please check how DC drive is controlled via CNC i.e. is it on Profibus or stand alone. If it is on bus you need to connect DI & run optimisation procedure.
OK. Does motor run in field weakning mode? What type of speed feedback is connected? tacho or encoder? Is it working OK. Please attach motor name plate details here.
OK. Have you checked DC motor armature commutator & brushes condition? Is it OK? Please check above points. |
Follow us on