10/20/2019 2:35 PM | |
Joined: 5/7/2018 Last visit: 12/16/2023 Posts: 25 Rating: (0) |
Ok, floor heating with two curves added to the diagram. Any comments about the diagram? I also could use some help with stopping the heatingpump when AI5 temp is over the setpoint Attachmentheatingsystem_2C.zip (189 Downloads) |
10/20/2019 4:03 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32843 Rating: (4061)
|
I tidied up your program a bit. For the heating pump, I have installed the following: What I do not understand in the burner control: Attachmentheatingsystem_2C_V2.zip (204 Downloads) |
This contribution was helpful to1 thankful Users |
11/13/2019 5:10 PM | |
Joined: 5/7/2018 Last visit: 12/16/2023 Posts: 25 Rating: (0) |
Hey again I finally had the time to install this system and now i have been testing and tweaking it for few days and it's working pretty good actually! I added some wirebreak/shortcut detection for the AI's, because I noticed that if I disconnect the AI4 ( Water TO the floor temp) sensor, it will give a -50c reading to the logo, which opens the 0-10V valve to 100% and let the tank temp water (45-95c) run directly to the floor and that would be really bad for my floors I also built a really ugly webserver to monitor the system. My question is, is there a way to get a reading with deecimal points to the web server? I'm reading some AM flags for the temperature, but I cant get proper reading out? Second question: Is there a way to adjust the reading that the PT100 gives? I think my sensors are giving bit low heat readings, is there a way to calibrate them? Thanks again :) Attachmentheating_system_13.11.19.zip (211 Downloads) |
Follow us on