11/14/2019 1:31 PM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585)
|
Hi, sorry I don´t know Gantner datalogger - will it workt with TCP IP or is it a profinet device? Then use Open User Communication Blocks like TSEND_C or TRECV_C or GSDML File. Check this for more information: With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols does the S7-1200 support?Regards, Towome
|
|
|
11/14/2019 1:45 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2684) |
Hello Pawlo; This webpage for Gantner instruments shows a download site for the gsdml files necessary to setup their Q series DAQ as a Profinet IO Device. https://www.gantner-instruments.com/?s=Profinet So yes, Profinet is available for some Gantner software. You have to find out if it applies to the product you want to use. Do you need more help to setup a Profinet IO Device on a IO Controller? Hope this helps, |
Last edited by: dchartier at: 11/14/2019 13:45:59 |
|
11/14/2019 3:33 PM | |
Joined: 9/27/2006 Last visit: 9/22/2024 Posts: 12282 Rating: (2684) |
Hello Pawlo; Here is a video tutorial using a Wago PLC as IO device on a S7-1200 IO controller; the steps are similar to what you will need to do. However, you will need somedocumentation from Gantner about the data exchange modules you need to select for yopur DAQ system. https://www.youtube.com/watch?v=Q_jOqL0Zp9s The steps are (briefly): - create a S7-1200 project and select your S7-1200 hardware - insert your Profinet gsdml file you downloaged from the Gastner site - select the Profinet address (TCP/IP addressing) and Profinet name for the DAQ system - select the modules you need for data exchanges between the S7-1200 and the Gantner DAQ - download the modifications to the CPU - start up communications. Hope this helps, Daniel Chartier |
Follow us on