11/14/2019 2:02 PM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326) |
The manual says the switch must be in "Vector" position :(see https://support.industry.siemens.com/cs/mdm/109757229?c=87359468555&lc=en-WW) "31118 - speed difference outside the tolerance range" indicates you have a general problem with the encoder. Check the parameters for the encoder inside the SINAMICS: When this is ok, you may look at the TO (e.g. with the Axis Control Panel) . |
|
|
This contribution was helpful to1 thankful Users |
11/16/2019 3:58 PM | |
Joined: 7/25/2018 Last visit: 4/8/2024 Posts: 47 Rating: (0) |
Hello Miami, Thanks for your help. I have already tried to run the motor using the drive control panel with a specified speed setpoint and I got good performance, so I did the same with a position setpoint using the technology object control panel where I also got some good performance. Doesn't that indicate that the parameterization of the technology object and the drive is correct?! |
Regards, Mohamad |
|
Follow us on