8/23/2018 9:57 AM | |
Posts: 2 Rating: (0) |
Hello, I want to change the parameter of an IO Link Sensor (PV7004 from IFM) but while the program is running. In case, i want to change the thresholds of the sensor. I'm using TIA Portal V13 with the ET200SP and the IO Link Master AL1103 (from IFM) See in attachment, the pictures of the project. I'm really, lost, i don't know what is not working. I've try to search for the error code but i found nothing. The goal is to recover the parameters, change what i want (more precisely threshold values) and then send back the data to the sensor. if there are few parameters to change i'll change to a direct transfer of the new thresholds, without recovering the data from the sensor. images attachment : [snip] Thank you in advance for your help Cordially, Clément Lévêque AttachmentScreenshots.zip (176 Downloads) |
Last edited by: Jen_Moderator at: 8/23/2018 12:46:20 PMRemoved links and added files as an attachment. |
|
8/23/2018 1:39 PM | |
Joined: 8/31/2005 Last visit: 8/20/2024 Posts: 2198 Rating: (328) |
The download page (https://support.industry.siemens.com/cs/ww/en/view/82981502) for IO-Link call says:
I think, you have to ask IFM for a similar block for their IO-Link Master. |
|
|
This contribution was helpful to1 thankful Users |
10/3/2018 4:52 AM | |
Joined: 5/8/2017 Last visit: 6/4/2020 Posts: 25 Rating: (2) |
Your index (551) should not be in hex. |
Follow us on