11/15/2019 1:26 PM | |
Posts: 8 Rating: (2) |
Hello I downloaded excel code Generator for TIA Portal Openness from here https://support.industry.siemens.com/cs/ar/en/view/109770550 I really like the idea. After install I have opened file Datenbase_automatic_Generation.xlsm I filled the blank fields In the Interface on the first sheet BaseSettings 1. I was not able to save this file. According to excel itself, the file has wrong Path. 2. Generation of code was not succesful after pressing Start generation button. It gave me one of two responses : Error 3004 or Error 429. According to debugger there might be an issue with writing to Error log and with ActiveX. Therefore I did following: I checked user rights on file Datenbase_automatic_Generation.xlsm I checked ActiveX in processes and Regedit. I checked .Net version I checked the syntax while filling BaseSettings I copied folder Temp from Anwendungsbeispiel project. I used Database_automatic_Generation.xlsm from Anwendungsbeispiel project. - None of these made my code generator working I am using Windows 10 Enterprise 2015 LTSB.,TIA 15.1., excel 2010 Please if you have any suggestion, how to make my code generator working. Thank you very much for your help :) |
Last edited by: Jen_Moderator at: 11/15/2019 13:44:15Optimized link. |
|
11/15/2019 8:18 PM | |
Joined: 9/8/2011 Last visit: 5/10/2024 Posts: 528 Rating: (84) |
Not sure, but try this: |
A smart person learns from their mistakes |
|
11/17/2019 2:04 PM | |
Joined: 7/28/2016 Last visit: 3/6/2024 Posts: 1 Rating: (0) |
Hello, I have exactly the same problem (Error 429)....did you solve your problem ? Best Regards Matthieu |
5/2/2020 10:08 AM | |
Posts: 10 Rating: (0) |
Please uninstall office 32 bit, and any other MS 32 bit applications. Install Office 64 bit, and you're done |
Follow us on