11/15/2019 11:40 PM | |
Posts: 2 Rating: (0) |
Hello everyone, I am experiencing this same issue with Step 7 as well, only it is the other way around. I have a project that is configured for the 2EK14 CPU, however I currently only have a 2EK13 controller on my bench. Dont care too much about the features that i am losing but i do care about getting online with the controller and it appears this is the only thing keeping me from doing so. I've already tried going into the HW configuration and "Replace Object..." on the CPU (Rack 0 Slot 1) however the selectable objects are not what i need. I am able to find the correct CPU in the library tree (317-2 PN/DP --> V2.6) to match the controller on the right hand side but I dont know how to replace the one that i currently have in Rack0 Slot 2. I've tried deleting but nothing happens it remains in Rack 0 slot 2. Any help would be appreciated. Thank you, -Luis T ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/18/2019 10:08:25New subject after splitting |
|
11/16/2019 12:01 AM | |
Joined: 9/16/2013 Last visit: 1/5/2024 Posts: 511 Rating: (105) |
Im using Step v5.5 + sp4, hardware catalog fully updated and I got both CPUs, I will post project for you with just CPU inside 2EK13 CPU . Check can you open it AttachmentS7_Pro9_.zip (34 Downloads) |
Website: |
|
Follow us on