11/15/2019 12:54 PM | |
Joined: 12/7/2018 Last visit: 10/7/2021 Posts: 4 Rating: (0) |
Hellow, can anybody answer?? |
11/19/2019 2:53 AM | |
Joined: 7/5/2013 Last visit: 4/26/2024 Posts: 3076 Rating: (505) |
Hello A.Fleyshman, when you are using SIMATIC HMI KTP400 Basic Color PN (6AV6647-0AK11-3AX0), then see description: SIMATIC HMI KTP400 Basic Color PN, Basic Panel, Key/touch operation, 4" widescreen TFT display, 256 colors, PROFINET interface, configurable from WinCC Basic V11 SP2/ STEP 7 Basic V11 SP2, contains open-source software, which is provided free of charge see enclosed CD So it is not possible to use WinCC flexible to create an application for that device. Regards, Frink |
Pi is exactly three! |
|
11/19/2019 5:28 AM | |
Joined: 7/5/2013 Last visit: 4/26/2024 Posts: 3076 Rating: (505) |
Hello A.Fleyshman,
no additional software required. See Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x (Video). Regards, Frink |
Pi is exactly three! |
|
Follow us on