11/19/2019 8:10 PM | |
Posts: 17 Rating: (0) |
Hi I need to change a 6ES7 416-2FK04-0AB0 by new one 6ES7416-2FP07-0AB0, Do I need to modify the HW or the CPU is plug and play? BR Alvaro ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/20/2019 09:56:45New subject after splitting |
|
12/9/2019 5:35 PM | |
Joined: 12/12/2018 Last visit: 7/1/2020 Posts: 34 Rating: (1) |
Yes you need to change in HWcnfg the old one by the new one |
Best Regards, |
|
12/9/2019 7:01 PM | |
Joined: 3/28/2015 Last visit: 4/14/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help: CPU 416F-2, MPI, PROFIBUS, 2,8 MBSuccessor product: 6ES7416-2FN05-0AB0 CPU 416F-2, MPI, PROFIBUS, 5.6 MBSuccessor product: 6ES7416-2FP07-0AB0 CPU 416F-2, MPI, PROFIBUS, 8 MBWhat should you watch out for when changing from one S7-400 CPU to another? You can replace the old CPU 6ES7416-2FK04-0AB0 With the second CPU successor 6ES7416-2FP07-0AB0 without modify the HW in the PLC program. |
Eng.Mohamed Ibrahim |
|
Follow us on