11/2/2022 11:45 AM | |
Joined: 3/15/2021 Last visit: 9/19/2024 Posts: 1 Rating: (0) |
Hello, Have you find solution for connection Siemens HMI to Allen Bradley Micro 850 PLC? |
6/5/2024 8:56 AM | |
Joined: 3/30/2020 Last visit: 9/20/2024 Posts: 4777 Rating: (981) |
I am also looking for the answer. But I do not have a Micro800 PLC in my hand to test. Part of the puzzle is the routing that must be specified. It is called the "CIP path". Information available in the software help is attached here for convenience. Another possible clue may be in a tutorial I came across which explain CompactLogix to Micro800 communications. [LINK: Message (MSG) – ControlLogix Writing Data Over Ethernet to a Micro800] This clue may however point to the fact that the communications to the Micro800 is not possible. I hope you share your information when you found some new information. AttachmentCIP path.pdf (178 Downloads) |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
Follow us on