11/20/2019 11:26 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Have you set drive parameters correctly? How much is the value in p2000? From PLC set point needs to scale between rpm to percentage value which needs to send to drive. Please refer below links which will help you to understand setting of parameters & establishment of communication. SINAMICS G/S: Speed control of a G120/S120 with S7-300/400 (STEP 7 V5) via PROFINET (PROFINET RT) SINAMICS G/S: Speed control of a G120/S120 with S7-300/400 (STEP 7 V5) via PROFINET (PROFINET RT) SINAMICS G: Speed control of a G120 using S7-300/400 (STEP 7 V5) with PROFIBUS (FW3.2) HTH |
Last edited by: Jen_Moderator at: 11/20/2019 12:29:23Optimized links. |
|
Follow us on