11/20/2019 1:29 PM | |
Joined: 3/23/2017 Last visit: 11/11/2021 Posts: 14 Rating: (0) |
I have used Modicon Modbus TCP driver to establish communication between WinCC and Mitsubishi FX5u (configured as Modbus Server). TIA program of WinCC RT and PLC program of Mitsubishi FX5U is attached. The communication is not working. The same configuration is working with Siemens S71200 PLC and Schneider M340 PLC which is also shown in the same TIA program. Please help me find the problem and suggest corrections, if any. P.S. >> I have tested Modbus communication of above mentioned PLC with modscan (client tool) and the communication works.AttachmentFiles.zip (310 Downloads) |
Follow us on