11/20/2019 9:18 PM | |
Joined: 1/26/2019 Last visit: 9/13/2023 Posts: 69 Rating: (1) |
Ahh, I felt so bad.. Always forgot to add the requirements, and clear instructions:: - TIA V15, WinCC Advanced Runtime, Win 10 O/S Question: I have a many rectangle control objects. They are perfectly aligned to the top. What is the best method to remove the space between these control objects. When the space are removed, the controls do not overlap, but are immediately adjacent to each other. Similiar function to this: https://docs.microsoft.com/en-us/office/vba/language/concepts/forms/adjust-horizontal-and-vertical-spacing-between-controls Currently, i am removing the spacing by determining the object width, and position y, one by one. |
Last edited by: GinkgoBoy at: 12/06/2019 05:59:41 |
|
Follow us on