10/9/2019 2:15 PM | |
Joined: 3/28/2010 Last visit: 9/18/2024 Posts: 1056 Rating: (213) |
diagram from the manual for 4 wire, 4-20mA wiring: signal (+) connects to I+ (terminal 2 in example) |
10/9/2019 2:36 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054)
|
hi vivky bhau, did you have a look in the manual of the module? SIMATIC ET 200SP analog input module AI 8xI 2-/4-wire BA the difference between 2-Wire and 4-wire-transducers is that the 2-wire-transducers have their power supply through the measurement-wires. Thats the reason why only 4..20mA-range can be used with it. hope this helps, regards, |
Last edited by: The Helping Hand at: 10/09/2019 16:34:20Optimized link. FCK WAR! |
|
Follow us on