11/11/2019 9:57 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please see the attached acreenshots. I need to change the PW for the user PTAuser on several machines in our plant. It is in a WinCC project that is integrated in a Simatic Manager project and the WinCC version in 7.4 Upd. 1 (we also have a few WinCC 7.0 but I will come to them later). We use VersionDog as our backup system. So I take out a copy of the running SW from VersionDog and change the PW in WinCC. Up to this stage it is working as it should. On another (WinCC 7.4 Upd.1) machine the download part also worked so the ES is capable of downloading to that version. Then I try to download the changes in WinCC to the HMI but on this machine I get the error message that " What goes wrong and how do I make this simple download AttachmentMissing RT Server.zip (27 Downloads) |
Last edited by: xmnj at: 11/11/2019 12:08:54Attachment |
|
11/13/2019 11:09 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hello schufri, Thank you for answering. I DID accept to open the project with the local computer as server but I did not make any changes on computername. On which computer should I set which computer name? I mean surely the WinCC server already has it's own name as server otherwise it would not be working or am I wrong? Should I set the computer name in the WinCC project on the ES to be that of the WinCC server I am going to download changes to? Furthermore I am wondering why the is not always the case when I went to download minor changes? - sometimes it works without anymore fuss after I give the initial yes. My projects are NOT PCS7 but S7 under Simatic Manager. The WinCC HMI projects are included with the PLC projects in Simatic Manager and the WinCC project is also (supposed to be) downloaded to the WinCC server with Simatic manager. Please see the attached screenshots.
AttachmentWCC DL.zip (23 Downloads) |
Last edited by: xmnj at: 11/13/2019 12:08:26 |
|
Follow us on