11/14/2019 11:27 PM | |
Joined: 11/12/2008 Last visit: 4/9/2024 Posts: 179 Rating: (16) |
Dear SOble, The module unconfigured module, I can n't change the the Input configuration. Thanks. |
HASSAN.S POJAILA |
|
11/22/2019 8:43 PM | |
Joined: 11/12/2008 Last visit: 4/9/2024 Posts: 179 Rating: (16) |
Hello, Here attached online monitor for PIW290, Also I have another problem, the value at OUT4 is not stable it's jumping, for example from 69 to 200 and so on, I did all isolating of sensor cable from any nearest power cable and I grounded the Simatic modules but still not stable. I connected Volt meter to the sensor transmitter, the value in voltmeter indicator was stable, kindly I'm looking for best solution because i'm using the AI module in scale sensor it's so sensitive and not accept any mistake value. Thanks AttachmentAI_Monitor.zip (46 Downloads) |
HASSAN.S POJAILA |
|
Follow us on