11/25/2019 7:58 AM | |
Joined: 3/8/2019 Last visit: 7/11/2024 Posts: 14 Rating: (0) |
Today I'm also facing this kind of problem. I have S7 300 CPU with CP 340 RS 232C Point to Point Communication Module. I am trying to send data to Epson Lx-310, I use P_Send Blocks for printing. At the moment I energized the blocks the txd and rxd indicator light in communication module is blinking for 4-5 seconds but the printer didn't print anything then after awhile the communication module sf light turn to red. I hope anyone here can help me with this problem. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/25/2019 13:33:25New subject after splitting |
|
11/25/2019 10:05 AM | |
Joined: 3/8/2019 Last visit: 7/11/2024 Posts: 14 Rating: (0) |
Hi Duris, Thank you so much to your response. 1. I didn't try to check my int data to printer, but later I download and install hercules application to check if it is working. 2. I want to print an int data type, like motor voltage, ampere and rpm. 3. I configured my communication module base on printer default communication settings that I have read in epson lx 310 manual. 4. What is SW? Do you mean what software I am using for programming. I use Tia Portal V13. 5. I attached below the diagnostic buffer from communication module and the construction of my program. Thank you very much. AttachmentJPEG.zip (100 Downloads) |
Follow us on