11/12/2008 10:57 AM | |
Posts: 15 Rating: (0) |
Hi, where i can download the trial version of Step - 7 software(version 5.4) |
11/12/2008 12:11 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hi No, you can't find here link to download Step7 (v5.4). If you want to use - must buy, If you want to study and training use STEP 7 Lite. ( Of course with some restrictions ). Available for free download as of immediately. Additional information is available in the Internet at: http://support.automation.siemens.com/WW/view/com/22764848 |
11/12/2008 1:54 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8740 Rating: (1168) |
Dear Dineshcs, Here is a link with MLFB number for ordering Trial license Step 7 professional: http://support.automation.siemens.com/WW/view/en/29746989 and here a link with MLFB number for ordering Trial license Step 7: http://support.automation.siemens.com/WW/view/en/22445076 Best regards, Wizard |
11/12/2008 3:05 PM | |
Joined: 9/23/2005 Last visit: 9/19/2024 Posts: 4347 Rating: (1446) |
Hi the service pack 3 for STEP 7 5.4 ( http://support.automation.siemens.com/BR/view/en/26578452) is free of charge and it is a full package. Naturally it comes without license. I don't know the dectails about of laws and user rights (please check it first!). In the practice, you can install it and use the automatic trial license to work for 14 days. |
Denilson Pegaia |
|
11/13/2008 5:18 AM | |
Posts: 15 Rating: (0) |
thanks all |
Follow us on