11/28/2019 11:15 AM | |
Posts: 7 Rating: (0) |
Hie all, I need to configure WinCC Advance RT to communicate as modbus master with multiple slave devices. Where i am able to read single device only. M finding difficulty to read Float data from other device. these are the modbus address and function code used. device 1 - Function Code: 4 : Input register Modbus address : 30071. ( this data not readable in WinCC) Device 2 - Function code: 1: Input Status modbus address : 10001. ( data Read in WIncc). M attaching few screen shots. for better understanding. P.S: device1 : energy meter, Device 2 : ICP CON DI module thanks in advance, Regards. AttachmentScreens.zip (36 Downloads) |
11/28/2019 1:18 PM | |
Joined: 6/19/2017 Last visit: 5/8/2024 Posts: 8016 Rating: (163) |
Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on