11/29/2019 9:34 AM | |
Joined: 9/10/2019 Last visit: 10/12/2023 Posts: 30 Rating: (0) |
Hello, How I can replace MM440 to S120 without profibus/profinet adress? Can you inform me how I can do this operation step by step? Thank you for information
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/29/2019 11:35:32New subject after splitting |
|
11/29/2019 10:09 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Yes it is possible. What is your application? Depending upon application, user can select compatible drive model from Sinamics series. CU are available for suitable function by which user can configure DI/DO & field interfaces & can run the application. Please refer below links for detail information or share details of your existing application so that forum member can help you. Type cancellation of MICROMASTER 4 family, effective Oct 1st, 2019 From MICROMASTER over to SINAMICS MICROMASTER 440, SINAMICS G120 (CU2x0x-2): Migration guideline HTH.
|
Last edited by: PISCEAN 2010 at: 11/29/2019 10:10:30Last edited by: Jen_Moderator at: 11/29/2019 11:38:23Optimized links. |
|
This contribution was helpful to1 thankful Users |
Follow us on