10/24/2019 12:24 PM | |
Joined: 2/24/2015 Last visit: 1/25/2023 Posts: 306 Rating: (75) |
Did you check on real hardware or on simulators? The simulator is working fine. |
11/8/2019 8:02 AM | |
Joined: 11/15/2012 Last visit: 4/1/2024 Posts: 143 Rating: (8) |
WinCC Advanced or Comfort Slider Problem When I try to create a faceplate including a slider, I found in following circumstance the slider would crash the runtime. (TIA Portal V15.1 upd3 in Win7.) When the dynamic “Tag for maximum “is 10 times large than static “Maximum scale value” (default is 100), the runtime will freeze and hang. It will bring unexpected behavior. Like “Maximum scale value” =100, “Tag for maximum” =1000. Also, when the dynamic Tag for maximum is changing, the scale mark will NOT change accordingly, its layout will stay with static maximum value. Please check with minimum value as well whether this similar problem exists. To avoid this problem, I had to set a very large value for default max value, but scale mark will not be visible in most cases. I also test slider in TIA Portal WinCC V15 Professional and WinCC 7.4 SP1, in their system, slider works well. Could you reproduce this problem? If you could reproduce, please report to Siemens, as I do not live in Germany right now, cannot contact the right person. WinCC Unified will come, please fix this problem, later TIA team may not put so much energy in old versions. I also posted a post before but not clearly described the problem, if someone could reproduce I will ask moderator to merge the topic. Best Regards. AttachmentWinCC Advanced or Comfort Slider Problem .docx (67 Downloads) |
Last edited by: C.Change at: 11/12/2019 08:32:31 |
|
11/13/2019 2:33 AM | |
Joined: 11/15/2012 Last visit: 4/1/2024 Posts: 143 Rating: (8) |
Could someone reproduce this problem? Please give some feedback when you have time. Thank you. Best Regards. |
Follow us on