11/29/2019 5:10 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
I have a suggestion here. 1. Get the installed software of the stations that are working. Start->all program-> siemens Automation->inst. Software 2. Get the system information export, run -> msinfo32.exe 3. Don't know the attached little tools helpful or not. Just for your extra info, the process running in the background. After you got all the system information and installed software, compared it with your local station. Make sure you are using the same pcs 7 versions. Then system information of the station can be a reference, as the setting of the language, region. AttachmentProcMon.zip (28 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on